Search FAQs
What’s the heat dissipation on the LRD range of overloads?
Please see the table below for heat dissipation on the LRD range of overload relays. For heat dissipation on the LRD overload relays with Everlink terminals, please see FAQ000233560.
Note: Power dissipated per pole
Reference | Setting range | Power dissipated in |
| | VA at Ith max. |
LRD01 | 0.1-0.16 | 1.33 |
LRD02 | 0.16-0.25 | 1.4 |
LRD03 | 0.25-0.40 | 1.38 |
LRD04 | 0.40-0.63 | 1.24 |
LRD05 | 0.63-1 | 1.55 |
LRD06 | 1-1.6 | 1.61 |
LRD07 | 1.6-2.5 | 1.67 |
LRD08 | 2.5-4 | 1.61 |
LRD10 | 4-6 | 2.14 |
LRD12 | 5.5-8 | 1.83 |
LRD14 | 7-10 | 1.77 |
LRD16 | 9-13 | 2.42 |
LRD21 | 12-18 | 1.99 |
LRD22 | 16-24 | 2.53 |
LRD32 | 23-32 | 2.43 |
LRD35 | 30-38 | 3.04 |
LRD3322 | 17-25 | 3.42 |
LRD3353 | 23-32 | 3.81 |
LRD3355 | 30-40 | 4.52 |
LRD3357 | 37-50 | 6 |
LRD3359 | 48-65 | 7.98 |
LRD3361 | 55-70 | 8.18 |
LRD3363 | 63-80 | 10.17 |
LRD3365 | 80-104 | 5.62 |
LRD4365 | 80-104 | 6.7 |
LRD4367 | 95-120 | 8.35 |
LRD4369 | 110-140 | 10.38 |
LRD33656 | 80-104 | 7.57 |
LRD33676 | 95-120 | 9.5 |
LRD33696 | 110-140 | 11.95 |
Note: Power dissipated per pole
Released for:Schneider Electric UK
Explore more
Explore more