Search FAQs
Can I have remote operation with RM6 RMU?
Remote operation can be enabled by integrating a RTU (Remote Telecontrol Unit) such as T200I or T200E and fitting actuators to the required functions. It may also be necessary to add additional wiring to enable the RTU to be integrated and commissioned prior to putting it back into service.
For more information on: -
- RM6 please click here
- T200E please click here
- T200I please click here
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: