Search FAQs
Can I have power factor correction capacitors inside Motorpact?
Yes, power factor correction capacitors can be incorporated into the Motorpact cubicle. They are usually located alongside the main contactor for: -
The size of capacitors will depend on the motor size and level of power factor correction required. The capacitors will be individually protected by HV fuses.
For more information on Motorpact please click here
- DOL starters
- Auto transformer starters
The size of capacitors will depend on the motor size and level of power factor correction required. The capacitors will be individually protected by HV fuses.
For more information on Motorpact please click here
Released for:Schneider Electric UK
Explore more
Explore more