{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the cabling diagram for the SR1CBL01 cable?

Article available in these languages: Czech, Greek

The SR1CBL01 is the programming cable to be use with the Zelio Relay SR1.

To be able to connect first generation Zelio programmable relays (part number SR 1xx) to a PC supporting the ZelioSoft programming software (part number SR1SFT01) you must have the SR1CBL01 programming cable.

The wiring diagram is as follows: Zelio connector end: brown: 2, yellow: 7, red: 3, orange: 5. PC SubD9 end: brown: 7, yellow: 2, red: 3, orange: 5.


ImagePinOut
Please Note: This cable and configuration is for the Zelio Logic First Generation - These items will not work with SR2 devices, Zelio Logic 2, or Zeliosoft2 Programing Software.



*********************************************************NOTE*******************************************************************
The Zelio SR1 software , devices and modules are discontinued. Please check the  Zelio Smart Relay SR2 or SR3.
***********************************************************************************************************************************

Schneider Electric UK

Explore more
Range:
Zelio Logic SR2/SR3
Explore more
Range:
Zelio Logic SR2/SR3
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.