Search FAQs
How can I use a motor protection circuit breaker type GV2, GV3, GV4, GV5, GV6 or GV7 with a single-phase load?
The GV range of motor protection circuit breakers (MPCB) can be used on a single-phase network by connecting 2 of the poles in series. In this way, all 3 motor protection circuit breaker poles are used.
NOTE The GV7 range is now obsolete, replaced by GV5 and GV6. Please visit our website www.se.com for further information.
NOTE The GV7 range is now obsolete, replaced by GV5 and GV6. Please visit our website www.se.com for further information.
Released for:Schneider Electric UK
Explore more