Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


This image can't be displayed


                     
                     
                     

                    Open Connectivity

                    Process Automation - PlantStruxure

                     
                     

                    PlantStruxure is built on open architecture technologies that allows transparent communications between field, process, plant and enterprise. Ethernet based network technologies and web services guarantee the efficient sharing and distribution of information between sensors, instrumentation, devices, automation controllers, operator workstations and other third party systems.

                    Your challenges

                    • Flexibility to update or expand the existing architecture
                    • Operate the plant smoothly and efficiently from any location
                    • The need for real time information to make the right decisions
                    • The need to identify the root cause of a problem as quickly as possible to minimise downtime
                    • The need to collect data to improve plant profitability and efficiency



                    Open Connectivity

                    Open Connectivity

                    Open Connectivity
                      
                     
                    Discover more

                    Discover more 

                    Additional support

                    Contact Schneider Electric
                    For additional help or to contact us, visit customer services
                     

                    Solution breakdown

                    Open Connectivity
                    Solutions based on universal technologies Ethernet TCP/IP and Web: Transparent Ready