Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Stand alone lighting control

                           
                           

                          Value proposition

                          Main Drivers
                          • Make savings controlling lighting consumption in the most simple way!

                          Solution in brief
                          • A simple yet efficient solution to optimise the lighting in buildings and offices using stand-alone electronics that provide simple automatisms based on three main parameters, alone or combined:
                            - time > timers devices
                            - intensity > dusks 
                            - presence > movement detection

                          Value proposition
                          • Compared to a traditional manual switch , here are typical energy savings a customer can achieved:
                            - Timer: potential savings up to 50% (stair-case)
                            - Dusks: savings can reach 50% (especially if combined with timer)
                            - Presence detectors: savings can reach 90% (oudoor application)

                          Differentiation factors
                          • For advanced indoor presences detectors - office PIR and/or building automation PIR -, heating/ventilation can be adjusted accordingly.
                          • For outdoor pressences detectors, outdoor lighting is turned on only when needed: upon the detection of movement but also only when the ambient light level is below a preset level. A light sensor in the PIR prevents the light from turning on if the daylight level is high enough.
                           

                          Main Energy Efficiency characteristics


                          Timer
                          • Placed between a light switch and the lighting device, the timer turns off the light automatically after a preset time.
                          • A socket outlet is connected to a timer (mechanically like a toggle switch) and is activated for a preset time only after the timer is pushed. Devices are no longer forgotten to be turned off.

                          Dusk
                          • A simple Dusk switch is inserted in the lighting circuit. For the advanced application with a timer, the timer is also inserted in the circuit.

                          Movement detection (PIR)
                          • Indoor PIR: A standard switch is replaced by a movement detector; lighting is turned on/off automatically upon detection of movement . For advanced PIR (office PIR and/or building automation PIR), heating/ventilation can be adjusted accordingly.
                          • Outdoor PIR: Outdoor lighting is turned on only when needed: upon the detection of movement but also only when the ambient light level is below a preset level. A light sensor in the PIR prevents the light from turning on if the daylight level is high enough.
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems:
                          • Timer flush: AT10, ATS10, ATC10, Unica, LK,...
                          • Dusk switch: Elux16, FC16, Argus
                          • Dusk switch: IC50, IC200, IC2000, IC2000P, IC Astro
                          • Timers: MIN, MINe, MINs, MINp,MIN3-3, MIN3-4