Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Staircase & Corridors Lighting optimization through timers

                           

                          Value proposition

                          Main drivers
                          • Building managers need to increase user comfort and save on lighting-related energy spendings.

                          Solution in brief
                          This solution enables to set lighting times to a minimum in passageways thanks to a timer making it possible to:
                          • Light one or several light sources from one or several control points,
                          • Keep lighting on for a pre-set time,
                          • Switch it off automatically.
                          • Override the timer for permanent lighting when necessary.

                          Value proposition
                          • Staircase timer allows reduction of energy spent for lighting. Instead of having the staircase and corridors permanently lit, the lighting is reduced to a pre-defined amount of time after one of the push-buttons connected to the timer is pressed.
                          • Without this timer solution, the light is often on permanently. With the timer, energy spent can be reduced by to 30 to 50% .
                           

                          Solution architecture

                          Solution architecture
                           

                          Main Energy Efficiency characteristics


                          In addition to significant energy savings, Automation provides:
                          • Greater comfort,
                          • Better security.
                          • Implementation is extremely simple.
                          • An up to 7-minute time delay can be set.
                          • The "override" function on the front face enables permanent lighting for cleaning and maintenance services.
                           
                           
                           
                           
                           

                          Solution breakdown

                          • Main Products & Systems
                            _
                            MIN timer
                            _ C60 type protection circuit-breaker.
                            _ CT contactor and its protection circuit-breaker if the power consumed is above 2 kW.