Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Simple metering solution for basic energy measurement

                           
                           

                          Value proposition


                          Main drivers
                          • It is the simplest starting point for users to start to understand their consumption. Once consumption is known then the most relevant areas for improving energy usage can be identified and other energy efficiency measures can be started.

                          Solution in brief
                          • This IEC solution is the most basic for energy measurement. Very simple meters are installed on relevant loads and users read the information from the display.

                          Value proposition
                          • After installing these simple meters, energy consumption can be tracked. Energy savings can be realized if you detect a source of over consumption in the installation .
                          • You can also identify, sector by sector, which is the largest consumer of energy.

                          Differentiation factors

                          • The installation is very easy . You just need some basics meters to be able to begin tracking your electricity consumption.
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Solution breakdown

                          • Main Products & Systems
                            _ Protection circuit breaker: Multi 9 C60
                            _ Instrumentation: meters ME4zrt, ME3zrt, ME1zrt, AMP, and VLT...
                            _ Current transformers: TI