Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Remote pumping optimal solution without programming

                           
                           

                          Value proposition

                          Main drivers:
                          • For simple remote pumping or booster stations based on 4 pumps.

                          Value proposition:
                          • Energy consumption is reduced by 20% to 30% on pumps according to their characteristics. Energy savings are easily estimated via ECO8 software.

                          Differenciation factors:
                          • Based on an Altivar 61 drive and its water solution card VW3 A3 503, t his optimal solution allows to easily manage pumps through one unique smart device, and without any programming.
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems: