Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Optimized Shop Windows Lighting through light sensitive switches

                           
                           

                          Value proposition


                          Main drivers
                          • Shop owners need to light up the shop window at nightfall and save energy by automatically switching off the lighting late at night when the streets are empty.
                          • They also want to prevent the lighting from switching on non-working days.

                          Solution in brief
                          • Programmable light-sensitive automatically switch shop-window lighting according to brightness and/or the time of the day.

                          Value proposition
                          • This solution provides significant energy savings by limiting the shop window lighting only when exterior lighting level is below a pre-defined threshold. Compared to permanent lighting, savings can go up to 50% of the energy consumption .
                          • In addition, IC 2000p+ increases energy savings by automatically extinguishing the lighting when there are fewer passers-by (late at night and on non-working days for instance). These additional savings could be as high as a further 25% when switching the light off from 11:00 p.m. to 05:00 a.m.
                           

                          Solution architecture

                          Solution architecture
                           

                          Main Energy Efficiency characteristics


                          In addition to significant energy savings, Automation provides:
                          • Excellent shop-window lighting as soon as night starts to fall.
                          • The shop-window is lit up after the shop is closed to allow window-shoppers to see the products on display.
                          • Implementation is extremely simple.
                          • The "override" function on the front face enables permanent lighting for cleaning and maintenance services.
                           
                           
                           
                           
                           

                          Solution breakdown

                          • Main Products & Systems
                            _ IC2000 P+ light sensitive switch associated with a wall-mounted cell
                            _ C60 type protection circuit-breaker
                            _ CT contactor and its protection circuit-breaker if the power consumed is above 2 kW.