Optimise swimming pool water management

Value proposition
Main drivers
Value proposition
Up to 25% energy saving thanks to the optimised management of swimming pool operation.
Possibility of temporary or continuous override operation (ON or OFF).
Automatic summer/winter time change.
Differentiation factors
Automated pool management via a dual-output programmable time switch .
Solution architecture
 | Circuit-breakers to protect the various devices The footbath water-filling solenoid valve is directly controlled by the IHP 2c switch contact The characteristics of protection circuit-breakers and CT contactor depend on the installed power and type of load
|
Main Energy Efficiency characteristics
The solution is to use IHP 2c programmable time switch:
To program on IHP 2c output 1; the days and times the pool water will be filtered
To program on IHP 2c output 2; the days and times the footbaths will be operational
Up to 6 years power backup in the event of mains failure.