Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Modular solution for pumping and additional treatment

                           
                           

                          Value proposition

                          Main drivers:
                          • For booster or complex pumping stations.

                          Solution in brief:
                          • Modular solution to manage more than 4 pumps and additional functions such as chlorination or tank management .

                          Value proposition:
                          • Based on Altivar 61 drives, this solution allows you to reduce energy consumption by 20% to 30% on pumps depending on their characteristics. Energy savings is easily estimated via ECO8 software

                          Differenciation factors:
                          • Flexible, this solution proposes high diagnostic capabilities thanks to Transparent Ready functionalities and its connexion to the Ethernet Network.
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems: