Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Manage ventilation in hotel bathroom

                           
                           

                          Value proposition

                          Main Drivers

                          • The hotel manager wishes to lower the electrical energy consumption while providing guests with maximum comfort by installing an automatic bathroom ventilation system.

                           

                          Solution in brief

                          • Ensure that the bathroom ventilation system is operational while the bathroom is in use and that it remains on only for a few minutes after the light has been switched off.
                          • A time-delay relay is used to prevent the extractor from switching off immediately and to ensure that it remains on during an adjustable time-delay period.

                           

                          Value proposition

                          • Peace of mind: Automation ensures considerable energy saving by automatically extinguishing lighting and ventilation when it is not necessary. Up to 15% of energy saving
                          • Flexibility: The time delay can be set from 0.1 second to 100 hours.
                           

                          Solution architecture

                           
                          Solution architecture
                          • The RTC relay supplies its output 18 as soon as input Y1 is activated
                          • The time delay starts when RTC input Y1 is disabled
                           

                          Main Energy Efficiency characteristics

                          The solution is to use an RTC relay to supply the extractor when the bathroom light is switched on:

                          • The ON-OFF switch controls the lighting and ventilation at the same time
                          • When the hotel guest switches off the lighting, the RTC relay continues to operate the ventilation
                          • The ventilator stops after a preset operating time to ensure that any unpleasant smells and moisture are removed but prevents energy waste.
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems: