Total Cost of ownership of a Low Loss Transformer compared to a standard manufactured Transformer is substantially lower when taking into account the losses incurred throughout the life time of the transformer.
As the unit cost of electricity has risen the return on investment has been significantly quicker.
Value proposition
ROI between 18 and 24 months
Internal transformer losses can be reduced by 20-25 % compared to standard manufactured Transformer.
Differentiation factors
Low Loss transformer are Cast Resin type Transformers. The used Technology is Schneider Electric patent.