Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Lighting control solution for outdoor/street lighting

                           
                           

                          Value proposition

                          Main drivers
                          • Public networks energy consumption management is a major concern for local communities

                          Solution in brief
                          • Lubio is a smart solution to management outdoor/street lighting efficiently.

                          Value proposition
                          • Lighting's supply tension, tension reduction during programmable periods of time and an astronomical clock enable a total management of energy consumptions.
                          • When Lubio is installed on a public lighting network equipped with High pressure Sodium lamps, the voltage regulation and reduction allows energy savings as high as 35%.

                          Differentiation factors
                          • The modularity of Lubio offers optimal flexibility for adapting to a highly diversified and scalable distribution network.
                          • Their small size and reduced weight guarantee far greater ease of maintenance
                          • Lubio integrates all necessary functions to manage public lighting:
                            - On/Off and lighting intensity management
                            - Low tension functioning periods.
                            - Main network's parameters measurement and monitoring.
                            - Savings calculation and Modbus communication
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems:
                             – DB90
                             – Lubio VRI 6 kVA