Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Injection press optimization through hydraulic clear mode solution

                           
                           

                          Value proposition


                          Main drivers
                          • The Energy Efficiency is based on the time left to the motor to run at low speed, called Hydraulic clear mode.
                          • During a production cycle, the motor is loaded less than 50% of the time. The energy saving will come from when the motor is not loaded (time of plastic cooling). When the motor is not loaded, is running at low speed (20Hz). 

                          Value proposition
                          • Profit from significant energy savings going up to 45%, by using the law of energy saving integrated into Schneider Electric variable speed drives.

                          Differentiation factors
                          • The Altivar 61 variable speed drive integrates a law of vectorial order controls which adjusts the magnetizing current according to the torque.
                          • The self-adaptation of the magnetizing current makes possible to get significant energy saving while profiting from the advantages of the vectorial control (optimization of the torque, compensation of slip)
                          • This law applies preferably to the loads with variable torque not requiring any particular dynamic performance (pumps and ventilations).

                          Example, 55kW-motor current:
                          40A current of idle run without variable speed drive
                          17A current of idle run with variable speed drive and the law of active energy saving
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems:
                            _ Pressure Sensor