Control lighting in classrooms

Value proposition
Main drivers
The training room fluorescent lights must come on when the presence of students in the room is detected, but only when the natural lighting is insufficient.
They must go off when the natural lighting is sufficient or as soon as the room is empty, leading to energy saving.
Value proposition
Automation ensures up to 20% energy savings.
Additional energy saving potential can be gained by including the heating or air conditioning in the system: example by using night economy when no movement is detected.
Differentiation factors
Thanks to the CDP ARGUS presence detector's lighting control, which is dependent on movement and brightness, only classrooms which are actually in use will be lit.
Solution architecture

10 A, AC 230 V, cos phi 0.6
Incandescent lamp max. 2300 W
Halogen lamp max. 2000 W.
The earthing system must be appropriate with the regulations in force in the country where the lighting is in use.
Main Energy Efficiency characteristics
The CDP ARGUS allows the lighting to be set from 10 to 1000 lux
It detects the slightest motions within a radius of 14 metres at a mounting height of 2.5 metres
Thanks to the 2 relay outlets not only the lighting but also the HVAC can be controlled with just one device
You can also manually switch the lighting ON and OFF at any time using a pushbutton.