Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Consulting solution to optimize pumping in a treatment plant

                           
                           

                          Value proposition


                          Main drivers:

                          • Boosting stations are very often using valves to adjust the pressure. When one valve is closed, 30% of the power is dissipated by the valve is around 50% of the power delivered by the motor.

                          Value proposition:

                          • Thanks to the drives, energy consumption is reduced here around 50% on boosting pumps.
                            Energy savings are easily estimated via ECO8 software.
                          • In this case the total cost saving (2 pumps) is 48K€ per year.
                            The investment is around 40k€ so the ROI is less than 1 year .

                          Differentiation factors:

                          • Based on an Altivar 61 drive and its water solution card VW3 A3 503, this optimal solution allows for managing pumping or booster stations based on 4 pumps through one unique device , and without any programming .
                           

                          Solution architecture

                          Solution architecture
                           

                          Main Energy Efficiency characteristics

                          • 2 Variable Speed Drives (VSD) (ATV-61HC13N4) to install on 132kW motors (2 motors). One runs in master mode and the other runs in slave mode. Make flow management by VSD. See the structure as below.

                          • 2 pressure meters installed to measure pressure on each pump.1 flow meter installed in the pipe. The 2 VSD (1 master, 1 slave) control the flow according to the process demand (this flow reference can be programmable). Pressure and flow can be adjust on site, or the pressure and flow signals can be transmited to control center, and be adjusted remotely.
                           
                           
                           
                           
                           

                          Solution breakdown

                          Main products & systems:
                              _ Drive water solution card: TE VW3 A3 503 (Altivar 61)
                              _ Instrumentation: Pressure meter
                          • Main services:
                             _ Maintenance contract for the Altivar
                             _ Training on the use of the System