Basic power monitoring system

Value proposition
Solution in brief
- A complete solution that provides easy customized access to electricity parameters of MV or LV switchboards through the Intranet and web pages.
Value proposition
- Up to 15% time and cost saving thanks to:
- Immediate access to diagnosis maintenance information
- Simplification of interfaces between products
- Continuous monitoring of quality and cost of power
- Reduce training for users
Differentiation factors
- Taking advantage of predefined web pages embedded in the panel, any authorised user regardless of their position - electrician, maintenance, manufacturing, site manager - can view valuable electrical information to save energy, avoid power outages or better manage the electrical asset.
- This solution includes delivering MV and LV power equipment that is ready to be plugged into the end-user's Intranet site. Access to the power equipment is done with Internet Explorer.
- This solution remains highly upgradeable. It can be considered as the basis for more advanced solutions to improve energy management one step further.
Main Energy Efficiency characteristics