Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                          Automated lighting in foyer cloakroom

                           
                           

                           

                          Value proposition

                          Solution in brief
                          • A simple and efficient solution based on 360° movement detector easely installed on the ceiling of the entrance hall.

                          Value proposition

                          • This solution provides a potential energy saving of 8% to 16%.
                          • Automatic control of lighting according to brightness level. A switch (optional) hidden from users' view, allows ON override of lighting if required.

                          Differentiation factors

                          • The absence of a light switch within reach of the public is more hygienic and ensures that the lighting is not switched on when it is not needed.
                          • Aesthetically pleasing and discreet appearance that makes it appropriate for all types of premises.
                           

                          Solution architecture

                          Solution architecture
                           
                           
                           
                           
                           

                          Key downloads

                           

                          Solution breakdown

                          • Main products & systems
                             _ Movement detector: MG CDM 360
                             _ Protection circuit-breaker: MG Multi9 C60
                             _ Flush-mounted switch (optional)
                             _ CT contactor and its associated circuit-breaker
                                if power consumption exceeds 1 kW.