Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                        Pumps & Fans Control (Industry/Infrastructure)

                        Pains & drivers

                        • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% of them control pump or fan applications
                        • Most pump and fan applications are driven by a DOL solution of SoftStarter. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge
                        • The CEMEP association has made a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year
                         

                        How can a customer manage energy more efficiently?

                        • To save energy you must:
                          - drive the motor with a frequency inverter instead of a contactor or Soft Start
                          - remove the restriction device (valve or damper)
                        • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
                        • The result is huge savings compared to conventional solutions:
                          - up to 50% for Fan , return on investment for the drive is within one year
                          - up to 30 % for a Pump , return on investment within 2 years
                         

                        Solutions or architectures used in the application

                         
                        Solutions or architectures used in the application
                        A) Solution without Drive
                        The motor turns at a fixed speed according to the network frequency and the number of poles.
                        Example : 3600 Rpm for 60 Hz
                        Motor 2 poles
                        The only way to adjust the Flow is a restriction device (damper) which generates losses.







                        B) Energy Saving Solution with Drive
                        The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
                        The Flow is directly proportional to the speed.
                        The damper or valve are no longer required.







                        C) Energy Consumption with and without Drive
                        Example for Fan Application

                        Outlet damper 
                        Variable speed drive 
                        50% of energy saving at 80% of the nominal flow


                        Example for Pump Application

                        Control valve 
                        Drive 
                        30% of energy saving at 80% of the nominal flow 

                         
                         
                         
                        Schneider Electric Solutions
                        Schneider Electric SolutionsFlexibilityProductivityEnergy cost savingInnovation


                        Altivar 61

                        ************


                        W@de W320i, Magelis XBT-N, TeSys U, Altistart 48, Multi 9

                        ******


                        W@de 320e, Magelis XBT-G, Vijeo Citect, Altivar 61

                        *****


                        Altivar 61, Magelis, Vijeo

                        *********


                        W@de RTU, Magelis XBT-N, Altivar 61, Multi 9

                        ********


                        Modicon M340, Advantys STB, FactoryCast, ConneXium, Altivar 61

                        **********


                        PowerLogic, Compact NS, Altivar 61

                        *********


                        Modicon Premium, Advantys STB, Magelis XBT, Vijeo, Altivar 61, TeSys U

                        **********


                        Modicon Quantum, PowerLogic PM650, Altivar 61, Altistart 48, TeSys LT6

                        **********


                        Altivar 61, Tesys U

                        n/an/an/an/a
                         
                          
                         
                        Discover more

                        Discover more 

                        Additional support

                        Contact Schneider Electric
                        For additional help or to contact us, visit customer services
                         

                        Customer testimonials