Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                        Lighting Control

                        How can a customer manage energy more efficiently?

                        • Lighting can represent up to 40% of energy consumption in buildings depending on segments
                        • Lighting control is definitely one of the easiest ways to save energy costs on one of the most common applications. Applying an effective lighting control solution, users can easily save up to 50% on their electricity bill compared to traditional ways
                         

                        Solutions or architectures used in the application

                        • The solution provides automatic means to optimise lighting based on the 3 main parameters indicated above (time, intensity and presence), alone or combined
                        • The solution can begin from very local and small solutions, such as timers, up to very sophisticated, customised but flexible, centralised solutions as part of building automation systems
                         
                         
                         
                        Schneider Electric Solutions
                        Schneider Electric SolutionsEase of InstallationEase of UsePotential SavingsIntegrated Supervisory Control


                        Multi 9 and Ultra Terminal wiring devices

                        ********n/a


                        IHP, Multi 9 C60

                        ********n/a


                        MIN, Multi 9 C60

                        ********n/a


                        CDM 360, Multi 9 C60

                        ********n/a


                        IC 2000P+, Multi 9 C60

                        ********n/a


                        CDP ARGUS, Vigi C60, C60N

                        n/an/an/an/a


                        TAC Vista

                        *********


                        Andover Continuum

                        *********