Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Energy Efficiency

                  Home Control

                  Pains & drivers

                  Pains & drivers

                  While comfort and safety are probably the most important selection criteria in home, energy efficiency, and the ability to reduce the "environmental footprint" of the house is getting more and more relevant.

                  Average breakdown of home energy consumption :
                  • Heating & Cooling: 60%
                  • Lighting: 14%
                  • Electrical applicances: 14%
                  • Hot water sanitary: 12%

                  How can a customer manage energy more efficiently?

                  Energy savings can be achieved through automating different functions of the regular daily life:
                  • Lighting control: turning off unnecessary lights sensing when nobody is in a room through presence detector, dimming the light intensity according to exterior lighting conditions, scheduling exterior lighting according predefined patters
                  • Heating, Ventilation and Air Conditioning¬†control: setting optimal temperatures for the different rooms of the house, Predefining heating/AC patterns in advance according to regular needs, remotely controlling heating/AC

                  Other functionalities can also improve energy efficiency:
                  • Alarm handling
                  • Preventive protection
                  • Remote control
                  • Multimedia control

                  Solutions or architectures used in the application

                  Home automation solutions are focused on the specific automation requirements of private homes and in the comfort and security of its residents. Usually, there are three main system architectures classified according to where the intelligence of the system resides:

                  • Centralised Architecture: a centralized controller receives information of multiple sensors and, once processed, generates the opportune orders for the actuators

                  • Distributed Architecture: all the intelligence of the system is distributed by all the modules that are sensors or actuators. Usually it is typical of the systems of wiring in bus

                  • Mixed Architecture: systems with decentralised architecture as far as which they have several small devices able to acquire and to process the information of multiple sensors and to transmit them to the rest of devices distributed by the house
                  Schneider Electric Solutions
                  Schneider Electric SolutionsFlexibilityProductivityEnergy cost savingInnovation

                  Altivar 61


                  W@de W320i, Magelis XBT-N, TeSys U, Altistart 48, Multi 9


                  W@de 320e, Magelis XBT-G, Vijeo Citect, Altivar 61


                  Altivar 61, Magelis, Vijeo


                  W@de RTU, Magelis XBT-N, Altivar 61, Multi 9


                  Modicon M340, Advantys STB, FactoryCast, ConneXium, Altivar 61


                  PowerLogic, Compact NS, Altivar 61


                  Modicon Premium, Advantys STB, Magelis XBT, Vijeo, Altivar 61, TeSys U


                  Modicon Quantum, PowerLogic PM650, Altivar 61, Altistart 48, TeSys LT6


                  Altivar 61, Tesys U