Water
  1. VerticalNavigation :

    The navigation will be updated automatically.

Water logo

Water solution: Optimised pumping for swimming pool

 
 

Value proposition

Main drivers

  • The private home-owner wants to save energy while optimising the water flow in his filtration system, keeping water moving for chemical dispensers and chlorinator efficiency.

 

Value proposition

  • At 80% of the flow, power consumption drops by 50% using a variable speed drive!
  • Up to 30% energy savings, optimising water flows for any application, filtration, cleaning, spa and heating...

 

Differentiation factors

  • Minimise the pump energy costs by operating at the lowest possible flow rate.
  • Place a variable speed drive Altivar 11 between the circuit breaker and the motor to achieve flow variation by electronically controlling the speed of the motor.
 

Solution architecture

Solution architecture
 

Main characteristics

The Altivar 11 drive combines all the functions that your application requires:

  • Reduction of energy consumption
  • Flow variation
  • Simplicity of use
  • Motor protection.
 
 
  
 
Discover more

Discover more 

Additional support

Contact Schneider Electric
For additional help or to contact us, visit customer services