Water
            Water logo

            Water solution: Optimise swimming pool water management

             
             

            Value proposition

            Main drivers

            • The swimming pool water must be filtered continuously on the days the pool is open
            • The water supply to the footbaths must only be operational during opening times.

             

            Value proposition

            • Up to 25% energy saving thanks to the optimised management of swimming pool operation.
            • Possibility of temporary or continuous override operation (ON or OFF).
            • Automatic summer/winter time change.

             

            Differentiation factors

            Automated pool management via a dual-output programmable time switch .

            • First output : control of the pool water filtering pump.
            • Second output : control of the footbath water supply solenoid valve.
             

            Architecture

             
            Architecture
            • Circuit-breakers to protect the various devices
            • The footbath water-filling solenoid valve is directly controlled by the IHP 2c switch contact
            • The characteristics of protection circuit-breakers and CT contactor depend on the installed power and type of load
             

            Main characteristics

            The solution is to use IHP 2c programmable time switch:

            • To program on IHP 2c output 1; the days and times the pool water will be filtered
            • To program on IHP 2c output 2; the days and times the footbaths will be operational
            • Up to 6 years power backup in the event of mains failure.
             
             
              
             
            Discover more

            Discover more 

            Additional support

            Contact Schneider Electric
            For additional help or to contact us, visit customer services
             
             
             
             

            Solution breakdown

            • Modular circuit-breakers up to 63A C60N
            • Programmable time switch: IHP 2c
            • Modular contactor 3 poles: CT