Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Water
            Water logo

            Water solution: Remote pumping optimal solution without programming

             
             

            Value proposition

            Main drivers:
            • For simple remote pumping or booster stations based on 4 pumps.

            Value proposition:
            • Energy consumption is reduced by 20% to 30% on pumps according to their characteristics. Energy savings are easily estimated via ECO8 software.

            Differentiation factors:
            • Based on an Altivar 61 drive and its water solution card VW3 A3 503, t his optimal solution allows easy management of pumps through one single smart device, and without any programming.
             

            Architecture

            Architecture
             
             
              
             
            Discover more

            Discover more 

            Additional support

            Contact Schneider Electric
            For additional help or to contact us, visit customer services
             
             
             
             

            Success Stories

             
             
            •   ...
            •   ...
             
             
             

            Solution breakdown

            Main products & systems: