Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Power Management
                           
                           
                           

                          SmartSwitch

                          Make a safe choice with SmartSwitch – the next generation in remote control panels

                           
                          SmartSwitch
                           
                           

                          SmartSwitch is an electronic remote control panel that allows the user to operate breakers on a switchboard from a safe distance, either away from the equipment, or outside of the switch room. SmartSwitch offers more features than standard hard-wired remote control panels:

                          • The ability to act as a central alarm panel for switchboard, showing detailed alarms from your Sepams.
                          • Keeping a record of when breakers are opened or closed by the operator.
                          • Events are recorded in an alarm summary.
                          • Graphical interface of the switchboard.
                          • A web page shows the same data as Schneider Electric’s Magelis HMI.
                          • The unit contains a back up battery to provide standby power for one hour.

                          To enhance SmartSwitch, there are a range of other options available including;

                          • 16 digital outputs, which can be used and configured for additional alarms in the switch room.
                          • SMS notification to a mobile phone when an alarm is present.
                          • Email notifications can be set up to alert you when an alarm occurs.
                          • The ability to interface with your Building Management System or SCADA

                          Contact us 

                            
                           
                          To know more

                          To know more 

                          Additional support

                          Contact Schneider Electric
                          For additional help or to contact us, visit customer services
                           

                          Case Studies