Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Power Management
                           
                           
                           

                          PC Mimic Diagram - PCMD

                          A simple approach to electrical network management

                           
                           

                          PC Mimic is a PC based software tool that allows a simple model of a customer’s electrical network to be created.

                          • Interactive mimic diagram enables users to gain and maintain familiarity with the distribution system for which they are responsible.
                          • Electrical status of sections of the network are immediately visible (live/dead/earthed/faulty).
                          • Observe the effects that operation of distribution switchgear have on the network.
                          • Use PCMD to rehearse the application of a safe system of work for both planned tasks (such as maintenance) and unplanned tasks (such as fault finding).
                          • Enables objective assessment of an individual’s competence in network operation.
                          PC Mimic Diagram
                          • Switching lists are prepared accurately and consistently with minimal effort.
                          • Easy editing of the network diagram to incorporate new equipment or to set up temporary arrangements.

                          Contact us 

                            
                           
                          To know more

                          To know more 

                          Additional support

                          Contact Schneider Electric
                          For additional help or to contact us, visit customer services
                           

                          Case Studies