RoHS Compliance
               
               
               

              RoHS Frequently asked questions

               
               

              RoHS Frequently asked questions

              1. What are the banned substances, and where are they found in EEE?

              The following 6 substances are banned:
              Lead, mercury, cadmium, hexavalent chromium, polybrominated biphenyls (PBB) and polybrominated diphenylethers (PBDE).

              These substances are used in Electrical and Electronic Equipment:

              • Mercury: in thermostats, sensors, relays in switches and discharge lamps
              • Lead: solder in printed circuit boards, glass in cathode-ray tubes and electric light bulbs
              • Cadmium: switches, springs, connectors, housings and printed circuit boards. (see below for more details)
              • Hexavalent chromium: Metal coatings for corrosion protection
              • Polybrominated biphenyls and polybrominated diphenyl ethers: flame retardants in printed circuit boards, connectors and plastic covers

              Cadmium is used by industry for numerous applications :

              • As an anti-binding agent (cadmium-plated parts have good lubricity)
              • As an anti-corrosive agent (particularly to protect connectors and fixings in conditions where electromagnetic compatibility (EMC) is a critical issue
              • As pigments and stabilisers in paints and plastics
              • As solders

               2. What are the thresholds below which it can be considered that a product complies with the RoHS directive?

              The thresholds to be allowed for are 0.1% by weight for lead, mercury, hexavalent chromium and PBBs and PBDEs. It is 0.01% by weight for cadmium, the homogeneous material in which the substance is located. 

                
               
              Discover more

              Discover more 

              Additional support

              Contact Schneider Electric
              For additional help or to contact us, visit customer services