Legislation
Safety Chain SelectorReduce cost and machine design time thanks to the help of our "Safety Chain Solutions"Schneider Electric provides you the means to get started on your machine adaptation of the new functional standards by using our certified ‘Safety Chain Solutions': a safety application example, based in a combination of interoperating products to realize a safety function, that includes an approved principle diagram and the correspondent safety level calculation. They allow you to save time and cost in obtaining the machine certificate according to the new European Machinery Directive by including it like a complementary documentation. They can be easily selected, according to your safety level and application required, by means of our safety selector tool. (*) Determination of the Performance Level requested (PLr)
(**) Categories of safety stopInternational standard EN/ISO 13850 specifies the functional requirements and design principles of emergency stop devices. It applies to all machines, whatever type of energy is used to control this function. The standard allows two types of stop:
The choice between these two stopping methods is determined by an evaluation of the machine-related risks.
|