Legislation
 
 
 

Inspection and testing

 
 

Part 6, chapters 61 to 63

During testing, to ensure the regulation has been complied with, precautions shall be taken to avoid danger to persons, property and installed equipment.

 

Residential Requirements

 
 

Example
The requirement for full inspection and testing has not changed, this should be carried out safely and by a skilled person. However, some details have changed and need to fully understood by the inspector.

What it means
Changes have been introduced such as: Inspection and testing Table 71A is now known as table 61.


Minimum installation values changed to:

  • 0.5 MΩ Selv or Pelv at 250 volts
  • 1.0 MΩ for systems up to and including 500 volts with a test voltage of 500 volts.
  • For systems above 500 volts tested at 1000 volts the minimum is also 1.0 MΩ


Solution
Only a skilled person competent in such work should be used to conduct the inspection and testing. Proof of competence should be shown.

 

 
 

Commercial Requirements

 
 

Example
The requirement for full inspection and testing has not changed, this should be carried out safely and by a skilled person. However, some details have changed and need to fully understood by the inspector.

What it means
Changes have been introduced such as:
Inspection and testing Table 71A is now known as table 61.

Minimum installation values changed to:

  • 0.5 MΩ Selv or Pelv at 250 volts
  • 1.0 MΩ for systems up to and including
    500 volts with a test voltage of 500 volts.
  • For systems above 500 volts tested at
    1000 volts the minimum is also 1.0 MΩ


Solution
Only a skilled person competent in such work should be used to conduct the inspection and testing. Proof of competence should be shown.

 

 
 
  
 
Discover more

Discover more 

Additional support

Contact Schneider Electric
For additional help or to contact us, visit customer services
 

The 17th Edition explained...

Read our bite-sized guides for a breakdown of the key changes within the 17th edition wiring regulations

  1. Scope of the BS7671:2008
  2. Definitions used in BS7671:2008
  3. Assessment of Characteristics
  4. Protection for Safety
  5. Erection of Equipment
  6. Inspection and Testing
  7. Special Installations
 

Take the mock test

Contact Schneider Electric

Take our free 
online mock test to see exactly how much you know about the 17th Edition.

 
 
 
 
 
 
 
 

17th edition training schedule

17th Edition training

Buy a copy of the 17th edition

Buy a copy