Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control

                            Sphere -  Wireless lighting systems

                            •  
                              Overview
                               
                            •  
                              Downloads
                               
                            •  
                              Support
                               
                            •  
                              FAQs
                               
                            Sphere
                            Benefits
                            • Control at the touch of a button
                            • Simple to install
                            • Controlled locally or remotely

                            Applications

                            • Private residential
                            • Offices
                            • Hotels
                            • Hotel rooms

                            Discovery

                             

                            Taking lighting control to a new dimension

                             
                             
                             
                            Description
                            Watch the Sphere Video

                            For homes and offices, Sphere offers the desirable prospect of sophisticated lighting at the touch of a button. Sphere functions through a coded wireless signal that is sent from a controller to wired-in receiver units. The receivers in turn control the light source, or other equipment connected to it, and can be discreetly located to ensure décor is not compromised.

                            • Enjoy a greater choice of scenes with the option of 5 or 8 channels. 
                            • Easy to install and simple to program.
                            • Combines control for both fixed and portable lighting. 
                            • Ability to control non light sources, such as extractor fans and garden water feature pumps. 
                            • Suitable for both new build and retrofitting. 
                            • Complements the Ultimate screwless flat plate range.
                             
                             
                             
                             5 channel Wall Controller

                            5 channel Wall Controller

                             

                            8 channel Remote Controller

                             

                            8 channel Remote Controller

                             

                            Relay, Mains and Fluorescent Dimmable Receivers

                            Relay, Mains and Fluorescent Dimmable Receivers


                            Back