Available in 400A and 600A ratings, the Shielded Heavy Duty Cut-Out goes beyond traditional cut-outs.
- Operator protection to IPXXB by using proven shielded fusegear technology
- Operator protection to IPXXB from live conductors as the cut-out incorporates segregated, flame retardant phase termination mouldings and a ‘through grip’ fuse handle on each fuse carrier
- Eight segmented phase termination modules on a common one-piece insulated base moulding
- The unit can easily be fitted in areas used by the general public as it conforms to IP4X
- Customers’ individual requirements can be accommodated by the use of additional accessories
- Conforms to ENA-TS 37-2, IEC 61439-1 and IEC 60529 standards