Electrical Distribution

Surge protection

 
Surge Protection
Description
Our modular range of low voltage surge protection devices suits the needs of both the residential, commercial & industrial sectors, meeting the international standard IEC 61643-11 class 2 test. This range comes in both fixed and withdrawable versions, 1 pole & multiple poles.