Electrical Distribution

Co-ownership -  Electric vehicle charging infrastructure for residences

  •  
    Overview
     
  •  
    Downloads
     
  •  
    Support
     
Electric vehicle charging infrastructure in a co-ownership residence car park
Benefits

Using an electric vehicle requires a safe and easy-to-use charging system. Schneider Electric has designed residential charging terminals in order to meet these requirements in the best possible way.

In a co-ownership residence car park configuration, the charging systems can be installed:

  • In personal parking garages or boxes, the terminal is connected to the existing individual electrical system or a line is routed from the flat.
  • In the case of unassigned parking boxes, common areas and the car park, the charging infrastructure is connected to the common area's electrical distribution system.

It should be noted that, in all cases, each circuit of the domestic station is protected by a earth leakage protection device.

Several co-owners or tenants have an electric vehicle although all may not have a garage. Also, frequent visitors with this type of vehicle are welcomed.

Free-standing terminals are available in the car park:

  • Private terminals: the user possesses an RFID badge for his/her own free-standing terminal. The user simply presents the badge to his/her terminal in order to use it. The free-standing terminal offers individual metering.

Common terminals: authorised individuals are issued with a personalised RFID badge which can used with any
free-standing terminal. The free-standing terminal sends the user's identifier and consumption to a server.

Discovery

 

Electric vehicle charging infrastructure in a co-ownership residence car park

 
 
 
Description

By installing a residential charging station, individuals benefit from equipment that is specifically designed to avoid electrical risks and help to manage their electricity consumption.

In a joint-ownership configuration, the charging systems can be installed:

  • In personal parking garages and boxes
  • In unassigned parking boxes, common areas and the car park

It should be noted that, in all cases, each circuit of the home charging station is protected by a earth leakage protection device and metering can be either on a common or individual basis. An identification command can also be added to operate the terminals.

Features:  charging command

  • On: immediate – as soon as the cable is plugged in or the Start button is pressed.
  • On: delayed – on an external order from a time switch or off-peak contact.
  • Off: automatic – battery fully charged; manual – by pressing the Stop button.

Technical characteristics

  • Frequency: 50/60 Hz.
  • Power: 3 to 22 KW
  • Depending on product, integrated surge protection device
  • Charging mode: Mode 3 as per IEC 61851
  • Charging socket-outlet: type 3 as per IEC 62196 and Schuko
  • Mechanical protection by sliding shutter

Installation architecture of an electric vehicle recharging infrastructure for electric vehicles in a co-ownership residence car park

> Learn more on our electric vehicle charging infrastructure 

 
 
 
 Electric vehicle charging station in a co-ownership residence car park

Electric vehicle charging system

 

Supervision of electric vehicle charging in a co-ownership residence car park

 

Supervision of electric vehicle charging in a co-ownership residence car park


Back