Qwikline II consumer units are fully type tested to BS EN 60439-3 and CM16 tests, which subject the units and incoming/outgoing devices to a 16kA through fault. They incorporate:
- unique plug-on MCB/RCBO fixing system, which guarantees a correct connection onto the busbar
- a rear clip which increases device security once plugged-on
- control devices that may be installed on any outgoing way
- incoming devices that can be ordered separately giving more than 1,000 combinations from just 46 references