The Domae range of consumer units offers the ultimate in terms of on-site flexibility at a very affordable price.
- The range offers consumer units and devices to help with compliance with the 17th Edition of the Wiring Regulations
- All Domae consumer units are fully type tested to BSEN60439-3
- The products benefit from a right hand incomer for easier installation where existing incoming cables fall on the right
- Front cover locking option on metal units
- Available in insulated or metal clad construction