Benefits
A range of safety control products which are simple to use and set up, with compact ergonomic products to meet requirements for starting or stopping motors.
Applications
All machines requiring : - DOL starting or stopping of motors
- load breaking of the machine control circuit
| |
Enclosed DOL starters, safety switch disconnectors, thermal-magnetic motor circuit breakers
|
|
| |
Description
TeSys wall-mounted DOL starters LG, LJ
- Enclosed DOL starters are used to control starting or stopping of the machine
- TeSys motor-starter solutions incorporate 2 auxiliary contacts which allow them to be integrated in safety wiring diagrams
TeSys Vario switch disconnectors
- Installed on an enclosure or in a cabinet, these rotary control switch disconnectors act as circuit load breakers
- Available in open or enclosed version
- Fixed on the front panel or DIN rail mounted
- Padlockable versions
Thermal-magnetic motor circuit breakers TeSys GV2-ME
| |
|
|
| |  TeSys model LG, LJ

TeSys GV2 ME
|