Automation and Control

                                  Variable speed drives - Medium Voltage

                                   
                                  Variable speed drives - Medium Voltage
                                  Description
                                  Range of medium-voltage variable speed drives from 0.5 to 10 MW.One of the most compact (up to 1.5 MW per metre of enclosure) and with one of the best efficiency levels on the market (~99%)
                                   
                                     
                                     
                                     
                                     
                                     
                                     
                                     

                                    Broken variable speed drive?

                                    Broken variable speed drive?

                                    For a fast and efficient repair service from the only approved repair centre for Schneider Electric drives, contact us now.

                                    Automation Solutions

                                    Automation solutions

                                    If your machine or process has been in service for an extended period of time, it may have undergone several modifications.