Automation and Control
  1. VerticalNavigation :

    The navigation will be updated automatically.

AS-Interface “Safety at work“ - Safety interfaces & I/O

Safety integrated in the networks

  •  
    Overview
     
  •  
    Downloads
     
  •  
    Support
     
  •  
    Part No. data
     
  •  
    FAQs
     
AS-Interface monitors and interfaces - AS-Interface “Safety at work“
Benefits

The simplification of the cabling combined with the level of diagnostics provided by AS-Interface « Safety at Work », favours the integration of safety functions to an existing AS-Interface solution.
No extra investment: your installation does not require the use of a safety PLC or a specific AS-Interface master.

Applications

All the installations requiring machine or operator protections, and using a AS-Interface network.

 

AS-Interface monitors and interfaces

 
 
 
Description
Safety monitors
  • Verifies correct operation of the AS-Interface system.
  • Monitors the safety devices connected to the yellow cable.
  • Available in 2 versions: with 1 or 2 safety outputs.
  • Configuration by software running under Windows, by simple Drag & Drop operation.
Safety interfaces
  • For dia 22 metal or plastic emergency stops Harmony.
  • For components with M12 output connectors.
  • For components with ISOM16 ou ISOM20 cable gland outputs.
 
 
 

Safety integrated in the networks


Back