A wide range of compact and robust products designed to operate in hazardous environments, mainly Dust zone 21 and 22.
Applications
What is an explosive atmosphere?
According to the Directive, it is the mixing with air, in atmospheric conditions, of flammable substances in the form of gas, vapour, mist or dust which, in the event of combustion, spreads throughout the non burning mix.
Inductive, Limit switches, Pressure control sensors for explosive atmospheres, OsiSense ATEX D
Description
Certified products, conforming to the European Directive ATEX94/9/CE