The screw limit switches are designed to monitor the movement of an object via an input drive.
The overtravel limit switches for power circuit switching are specifically designed to ensure the safety of hoisting equipment.
They directly break the power supply to the hoist motor if the load being handled accidentally exceeds the operating limits of the equipment.