CFL Factsheet
Mercury and compact fluorescent lampsFactsheetWhat are Compact Fluorescent Lamps (CFLs)? They are small fluorescent lights which fit into standard light sockets. They have longer lives and use less energy than a standard (incandescent) light bulb. Do CFLs contain mercury? Yes, they need mercury to generate light efficiently. The mercury is used to produce ultraviolet light, which is then changed into light we can see by a special coating in the lamp. The coating is inert and poses no health risk. Does this mercury pose a risk? The mercury cannot escape from an intact lamp and, even if the lamp should be broken, the very small amount of mercury contained in a single, modern CFL is most unlikely to cause any harm. How should I deal with a broken CFL? In the event of an accidental breakage of a CFL, normal good housekeeping is required. How should I clean up if I have broken a CFL on carpet? As mentioned earlier, the amount of mercury contained in a typical CFL is very small, up to 5 mg and is unlikely to cause any harm to human health. The level of risks involved in the case of a broken CFL on carpet is no greater than that on hard surfaces, although it may take a longer while to clean up the affected area due to the nature of the carpet surface. How should I dispose of the CFL waste? The bags can then be discarded through your local council. All local councils have to make arrangements for disposing of hazardous household waste. Many local authorities have a special place for hazardous household waste at a civic amenity site or household waste recycling centre. The National Household Hazardous Waste Forum runs a website with details of these centres for chemicals, but which also applies to other hazardous wastes (http://www.chem-away.org.uk/). Alternatively contact your local council direct. Further information on the environment and compact fluorescent lamps is available from the Defra website. Background information on mercury spills in residential settings is also available. Original HPA website link:
|