Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Panelbuilders
                           
                           
                           

                          The power of a standard adapted to your needs

                          Why you must use it!

                           
                           

                           The new IEC 61439-1&2 standard, the reference for safe and reliable Low Voltage switchboard 

                          IEC standards are now legal requirements or market benchmarks.

                          The new IEC 61439-1&2 is the benchmark for the construction of LV electrical switchboards.

                          IEC 61439 1&2 fully meets the requirements of designers and users of new generation LV switchboards:

                          • Safety of persons and equipment,
                          • Electrical availability,
                          • Long-term reliability and conformity.
                          To guarantee these essential values, the standard sets a wide range of requirements.

                          These include designing a “system” compliant in all aspects:
                          • Checking interactions and consistency between switchgear and equipment,
                          • Providing protection against electrical, mechanical and structural hazards,
                          • Simplifying system maintenance and upgrading cycles.
                           
                          The new IEC 61439 structure dedicates a section to assembly switchgear (IEC-61439-1&2) 
                          IEC 61439 -1&2* = Only "Tested assemblies"
                          General Rules 
                          IEC61439-1
                          Power SC Ass.
                          Distribution Boards
                          Construction Sites
                          Public networks
                          Busbar Trunking
                          • IEC61439-2
                          • IEC61439-3
                          • IEC61439-4
                          • IEC61439-5
                          • IEC61439-6
                          *IEC 61439-1&2 are published since January 2009, and IEC 61439-3 to 6 should be published in 2011.


                          The old IEC 60439
                          IEC 60439 -1 = "Type Tested" & "partially Type Tested"
                          General Rules + Type Tested Assemblies / Partially TTA
                          IEC60439-1
                          --------------------
                          Distribution Boards
                          Construction Sites
                          Cable Distrib. Cab.
                          Busbar Trunking
                           
                          • IEC60439-3
                          • IEC60439-4
                          • IEC6O439-5
                          • IEC60439-2
                            
                           
                          To know more

                          To know more 

                          Additional support

                          Contact Schneider Electric
                          For additional help or to contact us, visit customer services
                           

                          Products & Services