Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Panelbuilders
                           
                           
                           

                          10 functions to define the IEC 61439-1&2 standard

                           
                           

                          All the verifications proposed by standard IEC 61439 contribute to the achievement of 3 basic goals and 10 functions :
                          > The 5 Safety functions
                          > The 2 Continuity of service functions
                          > The 3 Compliance with end-user requirements functions

                          10 functions to define the new IEC standard 61439-1&2 : the 2 continuity of service functions 2 Continuity of Service functions

                           Maintenance and modification compatibility
                           Needs & design requirements Design verification Routine verification
                             
                          Capability to preserve continuity of supply without impairing safety during Assembly maintenance or modification.Through basic and fault protection and optional removable parts.
                          • IP tests
                          • Mechanical operation tests (especially for removable parts)
                          • Effectiveness of mechanical actuating elements
                          • Check protection of persons against electric shocks
                               
                           Electro-Magnetic Compatibility
                          Needs & design requirements Design verification Routine verification
                               

                          Properly function and avoid generation of EMC disturbances by incorporating electronic devices complying with the relevant EMC standard, and their correct installation.

                          • EMC tests according to product standards or generic EMC standards

                          None

                            
                           
                          To know more

                          To know more 

                          Additional support

                          Contact Schneider Electric
                          For additional help or to contact us, visit customer services
                           

                          Products & Services