Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Control Panel
Panelbuilders' icon
 
 
 

Incoming protection & switching

Click on the product reference to access to further information

 
 
 
 
 
 
 


Function

Switch
disconnector

Switch Fuse disconnector

Circuit-breaker

Isolation & Disconnection

¤

¤

¤

Switching

¤

¤

¤

Protection

 

¤

¤

 

Range


Tesys Vario


Interpact


Tesys GS

C60/NG

Compact

Masterpact

         

 

 

Rated operational current (A) 

12 to 175

40 to 2500

32 to 1250

10 to 125

100 to 1600

800 to 6300

Number of poles

3 to 6

3 to 4

Short circuit making capacity at 400V Icrn (kA)

0,5 to 3

50 to 220

5 to 90

10 to 50

36 to 150

42 to 150

References

V 

INS

GS

C60/NG125 

NS

NT or NW

 

> Click on the desired product reference to access information

  
 
To know more

To know more 

Technical guides

Brochure picto
 

Software (free download)

Flat screen picto
 

 
   
 
 

Back to the control panel homepage