Original Equipment Manufacturers
  1. VerticalNavigation :

    The navigation will be updated automatically.

 
 
 

Success stories - HVAC & R

 
 

Refrigeration system integrator (Canada)

   A Canadian refrigeration system integrator sought to improve energy conservation through a decentralised system to independently control temperatures. The installation would have to incorporate an easy programming tool for simplified communication, as well as ease of implementation and maintenance.

Benefits
- 22% energy saving for the end user
- Reduced overall wiring and product cost
- Direct communication between the independently controlled cold producer, tank and unit

Main customer requirements

Operating energy cost reduction
- Decentralised automated system architecture
- High-performance regulation functions
   

Overall solution cost reduction
- Reduced wiring time
- Reduced installation errors
- Reduced equipment costs

Improved communication network performance
- Communication of all systems with central supervision for monitoring and configuration functions

Our answer
An open, flexible solution featuring the Twido Compact controller, Ethernet and the PT100/PT10008-input temperature extension module delivers:
- Eight inputs instead of the usual four
- Ethernet connectivity for direct communication

  
 
Discover more

Discover more 

Additional support

Contact Schneider Electric
For additional help or to contact us, visit customer services