Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Water
              Water logo

              Reference: Water

              Wastewater treatment plant, Csepel (Hungary)

              The largest European Union wastewater treatment plant treats 95% of its wastewater

              Reference: Water 

              95% of wastewater treated instead of 54%.

              15% reduction in design cost

               

              I. CUSTOMER ENVIRONMENT / PROJECT CONTEXT

               

              Customer profile:

              Genesis of the project
              Today in Budapest, Hungary, 600 000 m3/day of wastewater is discharged into the Danube. 46% of this water is not treated at all.
              In 2002, Hungarian Program for Treatment of Waste Water specified that Budapest City has to comply in 2010 with the objectives of the 1994 Sophia Convention, which aimed at the protection of the Danube. The treated water has to comply with EU standards.
               

              Customer objective and constraints:

              Customer objective

              The two objectives of the city involve the construction of a plant capable of treating effluents generated by a population of 1,5 millions habitants.
              Veolia and Suez are leading the consortium designing this wastewater treatment plant with a capacity of 350000 m3/ day, the largest of the European Union. For this, the consortium needs a unique partner taking the full responsibility of the process and energy management solution completion: Schneider Electric.
               

              II. SOLUTION IMPLEMENTATION

               

              Solution overview (services, products, systems, architectures...):

               

              A turnkey solution

              Complete study and design of the architecture.

              • Project management
              • Standardization and objects library creation
              • Full delivery and commissioning of motor control, process automation and energy efficiency from medium voltage to low voltage.

              The upstream collaboration with Schneider Electric at the design stage allows standardisation and minimizes the risks all along the project.

              Schneider Electric's added value

               

              • Schneider Electric is a global company well implanted in Hungary. Furthermore, Schneider Electric is a key and regular partner for Veolia and Suez.
              • Schneider Electric has a Customer Interface. By fully managing the key steps of the project (provides a turnkey ED and Automation Scope for the project), Schneider Electric insures a single point of contact for the customer.
              • Deep technical involvement - not only limited to products but mainly focused on applications and projects.
               

              III. RESULTS / ACHIEVEMENT

               

              Customer benefits:

              + By reaching 95% of wastewater treated instead of 54%, Budapest City will comply with European Union regulation

              + The new wastewater treatment plant will allow Energy efficiency

              + Schneider Electric allowed 15% design cost reduction

               
               
                
               
              Discover more

              Discover more 

              Additional support

              Contact Schneider Electric
              For additional help or to contact us, visit customer services