• Default Alternative Text
    For shopping malls, high-rise commercial buildings, tunnels, etc.

    SAFETY STANDBY GENERATOR DEDICATED SOLUTION

Default Alternative Text

Challenges

Protecting and switching standby generation in large commercial buildings

Commercial buildings need constant power and a reliable backup plan in the event of a potentially dangerous and disruptive outage. Building codes may also place special requirements on the electrical system. A standby generator will supply lights and safety equipment until service is restored.

Our experts help you throughout the entire generator life cycle

Illustration, Machine LifecycleSolutions, Industrial production, machine control.
  • Solutions

    • Continuity: Selectivity of Compact or Masterpact circuit breaker, with Micrologic trip unit ensures safety in the event of a fault. In those occurrences, only the breaker closest to the fault trips.
    • Safety: A coordination study of protection and switching devices ensures equipment withstands short-circuit currents without damage.